SBOA630 June 2025 AMC7836 , DAC61408 , DAC61416 , DAC71408 , DAC71416 , DAC7714 , DAC7715 , DAC7724 , DAC7725 , DAC81408 , DAC81416 , OPA206 , OPA2206 , OPA4206 , TPS2661 , TVS3301
| Key Input Parameter | Key Output Signal | Recommended Devices |
|---|---|---|
SPI or I2C communication to control DAC voltage output | ±10V output DAC signal with overvoltage protection | DAC81408, OPA206, TPS26611, TVS3301 (optional) |
Objective: Protection of a ±10V signal from a sustained ±32V connection for a digital-to-analog converter (DAC) that does not have a positive sense pin.
This circuit design describes an overvoltage protection circuit for a precision DAC output. This circuit protects the DAC output from a continuous overvoltage above the maximum and below the minimum supply voltages. In a device without a positive sense pin, the DAC output buffer is contained within the device, without pin access to the positive sense feedback pin of the output buffer. The overvoltage protection circuit consists of an op amp set up in unity gain, an eFuse to protect the output, and an optional transient-voltage-suppression (TVS) diode. For a DAC operating on ±15V, the output is protected to ±32V or greater without damaging the DAC and the protection circuit. This type of protective circuit buffer can be used in many industrial factory automation and control applications. This circuit is particularly useful if the output experiences an overvoltage event from miswiring at an output terminal such as in a Programmable Logic Controller (PLC).
The overvoltage protection buffer is simulated with PSpice®. First, the transfer function of the buffer is simulated using a pulse voltage source as the DAC. The input of the buffer is ramped from –10V to +10V, showing the full output range of the DAC. The buffer schematic is constructed for simulation.

The transfer function from input to output of the buffer is derived from the transient simulation.
A second transient simulation shows the current during an overvoltage event.
The input is set to 0V and a voltage supply is placed at the output of the buffer. The supply ramp simulates the transition from –32V to +32V.
The simulation begins with the output at –32V, the TPS26611 eFuse is open, preventing any current from being sourced from the output of the OPA206. The residual current comes from the input of the OPA206 which has an integrated input protection, limiting the current to about 5mA. The current seen at the output of the buffer remains at 5mA as the voltage is reduced.
As the voltage increases to near the lower supply voltage of –15V, the TPS26611 begins to conduct current from the OPA206 output. The OPA206, driven by the ramping voltage, immediately reaches the device current limit of 30mA. This current limit is lower than the 32mA current protection level of the TPS26611, and allows the conducted current. The OPA206 sustained current limit is not destructive.
The ramped voltage rises and passes 0V and the output of the OPA206 changes from sourcing current to sinking current. The OPA206 is forced into a 30mA current limit in the opposite direction.
Finally, the ramped voltage rises above the positive supply of +15V. The TPS26611 eFuse opens again and the OPA206 output stops sinking current. Here, the only output current comes from the OPA206 input protection.
The TVS3301 is not simulated. However, the output is not sent above the protection threshold of 33V, which turns on TVS conduction. At the simulated level of 32V, TVS3301 does not affect the operation of the protection buffer and output of the DAC.
The overvoltage protection buffer is constructed for testing and is attached to the output of the DAC81416-08EVM. First, the output of the DAC is ramped from –10V to 10V to drive the buffer input. The offset seen from the buffer is measured to be less than 10µV over the full range.
The output is then connected to a variable supply. As the output is driven, the current at the output is recorded. The measurement starts with the supply at –32V and the variable supply is raised to +32V. Then the output is changed from +32V back down to –32V. This setup is similar to the schematic in the previously described simulation.
In the test, the OPA206 short-circuit current and input protection current are slightly lower than simulation. There is a hysteresis in the closing and opening of the TPS26611 eFuse. When starting with the TPS26611 eFuse closed and conducting current in normal operation, the eFuse opens when the output rises and is driven to about 2.5V beyond either supply. Here, the TPS26611 shuts off when the output is forced up above 17.2V or below –17.5V. This is partially seen in the simulation, which was run with a single ramp from a low to a high voltage.
The following table shows an example register map for this application with the DAC81408. The values given here are for the design choices made in the Design Notes section.
| Register Address | Register Name | Setting | Description |
|---|---|---|---|
| 0x03 | SPICONFIG | 0x0A84 | [15:12] 0b0000: Reserved |
| [11] 0b1: Thermal alarm triggers the ALMOUT pin | |||
| [10] 0b0: ALMOUT is not set between DAC updates | |||
| [9] 0b1: CRC error triggers the ALMOUT pin | |||
| [8:7] 0b01: Reserved | |||
| [6] 0b0: Soft toggle operation disabled | |||
| [5] 0b0: Device is in active mode | |||
| [4] 0b0: CRC is disabled | |||
| [3] 0b0: Streaming mode is disabled | |||
| [2] 0b1: SDO pin is operational | |||
| [1] 0b0: SDO updates during SCLK rising edges | |||
| [0] 0b0: Reserved | |||
| 0x04 | GENCONFIG | 0x3F00 | [15] 0b0: Reserved |
| [14] 0b0: Internal reference enabled | |||
| [13:6] 0b11111100: Reserved | |||
| [5:2] 0b0000: Differential mode disabled for all channels | |||
| [1:0] 0b00: Reserved | |||
| 0x09 | DACPWDWN | 0xF00F | [15:12] 0b1111: Reserved |
| [11:4] 0b00000000: All channels enabled, not in power-down mode | |||
| [3:0] 0b1111: Reserved | |||
|
0x0B, 0x0C |
DACRANGE0 (Channels 7:4), DACRANGE1 (Channels 3:0) |
0xAAAA | [15:12] 0b1010: Set the DAC output range to ±10V |
| [11:8] 0b1010: Set the DAC output range to ±10V | |||
| [7:4] 0b1010: Set the DAC output range to ±10V | |||
| [3:0] 0b1010: Set the DAC output range to ±10V | |||
|
0x14 – 0x1B |
DAC0–DAC7 (Channels 0:7) |
0x8000 |
[15:0] Set DAC data code for output voltage of 0V |
The following shows a pseudocode sequence to initialize the setup for the DAC81408. This pseudocode sets up the device for one channel for an output of ±10V. The values given here are for the design choices made in the Design Notes section.
Pseudocode Example for DAC81408
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Set the device in active mode
3: WRITE SPICONFIG(0x3), 0x0A, 0x84
4: //Enable the internal reference
5: WRITE GENCONFIG(0x04),0x3F, 0x00
6: //Enable all DAC channels, not in power-down mode
7: WRITE DACPWDWN(0x09), 0xF0, 0x0F
8: //Set Channels 7 to 4 to ±10V output range
9: WRITE DACRANGE0(0x0B), 0xAA, 0xAA
10: //Set Channels 3 to 0 to ±10V output range
11: WRITE DACRANGE1(0x0C), 0xAA, 0xAA
12: //Set DAC0 to output 0V
13: //Data is configured in straight binary, not two's complement notation
14: WRITE DAC0(0x14), 0x80, 0x00
15: //Channels 1 through 7 configured through registers 0x15 - 0x1B
Find other possible devices using the Parametric search tool.
| Device | Key Features | Link |
|---|---|---|
| DAC81408 | 8-Channel, 16-Bit, High-Voltage Output DACs with Internal Reference | DAC81408 |
| OPA206 | Input-Overvoltage-Protected, 4µV, 0.08µV/°C, Low-Power Super Beta, e-trim Operational Amplifiers | OPA206 |
| TPS26611 | 50V, Universal 4–20mA, ±20mA Current Loop Protector With Input and Output Miswiring Protection | TPS26611 |
| TVS3301 | 33V Bidirectional Flat-Clamp Surge Protection Device | TVS3301 |
See Analog Engineer's Circuit Cookbooks for TI's comprehensive circuit library.
Additional Resources
For direct support from TI Engineers, use the E2E community: