SBOK029D April   2018  – November 2023 TMP461-SP

 

  1.   1
  2.   TMP461-SP Single-Event Effects (SEE) Radiation Test Report
  3.   Trademarks
  4. 1Overview
  5. 2SEE Mechanisms
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 SEL Results
    2. 5.2 SET Results
    3. 5.3 Event Rate Calculations
  9. 6Summary
  10.   A Confidence Interval Calculations
  11.   B References
  12.   Revision History

SEL Results

During SEL characterization, the device was heated using forced hot air, maintaining the die temperature at 125°C. The temperature was monitored by means of a K-type thermocouple attached as close as possible to the die. The species used for the SEL testing was a Praseodymium (59Pr) ion with angle of incidence at 0° and 25° for an LETEFF = 76.18 MeV-cm2/mg and 65.65 MeV-cm2/mg. The kinetic energy in the vacuum for this ion is 0.885 GeV (15-MeV/amu line). A flux of approximately 105 ions/cm2-s and a fluence of approximately 107 ions were used for all seven runs. The VCC voltage was set to the recommended maximum at 3.6 V. Run duration to achieve this fluence was approximately two minutes. No SEL events were observed during all four runs shown in Table 5-1. Figure 5-1 shows a plot of the current versus time.

Table 5-1 TMP461-SP SEL Conditions Using 59Pr With Angle-of-Incidence = 0° and 25°
RUN #DISTANCE
(mm)
TEMPERATURE
(°C)
IONANGLEFLUX
(ions·cm2/mg)
FLUENCE
(# ions)
LETEFF
(MeV.cm2/mg)
2340125Pr25°1.00E+051.00E+0776.18
2440125Pr25°1.00E+051.00E+0776.18
2540125Pr1.00E+051.00E+0765.65
2640125Pr1.00E+051.00E+0765.65

No SEL events were observed, indicating that the TMP461-SP is SEL-immune at LETEFF = 76.18 MeV-cm2/mg and T = 125°C. Using the MFTF method described in Appendix A and combining (or summing) the fluences of the seven runs (4 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated as:

σSEL ≤ 1.84 × 10–7 cm2 for LETEFF = 76.18 MeV-cm2/mg and T = 125°C.

GUID-FAC4002B-6F02-4827-9E8C-628E8C5B4B91-low.pngFigure 5-1 Current vs Time (I vs t) Data for VCC Supply Current During SEL Run #23