SBOU128B february 2013 – july 2023 INA231
The Calculation tab, as shown in Figure 5-10, allows the user to follow the software flow with basic calculations performed from within the device. It is important to note that the calculations are performed with the decimal values of the corresponding registers.
Figure 5-10 Theory of Operation Flowchart on the Calculation Tab