SFFS624 March 2024 MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0G3507-Q1
The message RAM in MCAN module stores computes check bits (ECC bits) for each word of data stored. An ECC memory always protects against single-bit errors in the data. Address decode logic for the memory is not covered by the memory ECC logic. There is an ECC aggregator module inside the module that aggregates status from the ECC memories into a single interrupt to the host. The aggregator also supports software readable status of ECC single/double-bit errors and associated info such as RAM address and data bit(s) that are in error.