SLAAE88B December 2022 – March 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The MCU host firmware contains an image of the target application as a header file(application_image.h). The header file is the new application firmware that need to programed into the MSPM0 target device. To get the header file, there is a conversion utility in the GUI MSPM0_BSL_GUI.exe in the following path:
< …\mspm0_sdk_xxxx\tools\bsl\BSL_GUI_EXE >.