SLAAE88B December 2022 – March 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
If the private protocol is needed, the ROM-based BSL core cannot be used any more and the secondary BSL demo can be referred. A totally open sourced secondary BSL demo is provided in the SDK that you can use to easily modify the protocol. The default protocol of the secondary BSL demo is the same with ROM-based BSL.
There are also two kinds of secondary BSL demos mentioned, as shown in Figure 1-6. Use MSPM0G3507 as an example: