SLAAED1G May   2023  â€“ August 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Overview
  5. MSPM0 Online Selection
  6. Software Development Instructions
    1. 3.1 Key Documentation
    2. 3.2 LaunchPad Setup
      1. 3.2.1 Debugger Selection
      2. 3.2.2 LaunchPad Introduction
    3. 3.3 MSPM0-SDK Setup
      1. 3.3.1 MSPM0-SDK Installation
      2. 3.3.2 MSPM0-SDK Introduction
        1. 3.3.2.1 Examples Folder Introduction
        2. 3.3.2.2 Documents Folder Introduction
    4. 3.4 SysConfig Setup
      1. 3.4.1 SysConfig Installation
      2. 3.4.2 SysConfig Introduction
        1. 3.4.2.1 Basic Concept
        2. 3.4.2.2 Project Configuration View
        3. 3.4.2.3 Board View
        4. 3.4.2.4 NONMAIN View
        5. 3.4.2.5 SYSCTL View
        6. 3.4.2.6 Peripherals Setup
    5. 3.5 IDE Quick Start
      1. 3.5.1 CCS Quick Start
        1. 3.5.1.1 CCS Installation
        2. 3.5.1.2 Import a SDK Example
        3. 3.5.1.3 Example Download and Debug
        4. 3.5.1.4 Migrating Between MSPM0 Derivatives
        5. 3.5.1.5 Generate Hex Files
        6. 3.5.1.6 Program NONMAIN
      2. 3.5.2 IAR Quick Start
        1. 3.5.2.1 Environment Setup
          1. 3.5.2.1.1 SDK Support Setup
          2. 3.5.2.1.2 SysConfig Support Setup
        2. 3.5.2.2 Import a SDK Example
        3. 3.5.2.3 Example Download and Debug
        4. 3.5.2.4 Migrating Between MSPM0 Derivatives
        5. 3.5.2.5 Generate Hex Files
        6. 3.5.2.6 Program NONMAIN
      3. 3.5.3 Keil Quick Start
        1. 3.5.3.1 Environment Setup
          1. 3.5.3.1.1 MSPM0 CMSIS-Pack Setup
          2. 3.5.3.1.2 Sysconfig Support Setup
        2. 3.5.3.2 Import a SDK Example
        3. 3.5.3.3 Example Download and Debug
        4. 3.5.3.4 Migrating Between MSPM0 Derivatives
        5. 3.5.3.5 Generate Hex Files
        6. 3.5.3.6 Program NONMAIN
  7. Hardware Design Instructions
    1. 4.1 Obtaining a MSPM0 Package
    2. 4.2 Fix Pin Functions through Sysconfig
    3. 4.3 Schematic and PCB Attentions
  8. Mass Production Instructions
    1. 5.1 Generate Production Image
    2. 5.2 Program Software Tools Quick Start
      1. 5.2.1 Uniflash Quick Start
        1. 5.2.1.1 Program Through SWD
        2. 5.2.1.2 Program Through Bootloader
        3. 5.2.1.3 Program Through CMD Line Interface
      2. 5.2.2 JFlash Quick Start
      3. 5.2.3 C-GANG Quick Start
    3. 5.3 Program Hardware Quick Start
  9. Quality and Reliability Instructions
    1. 6.1 Quality and Reliability Material Entrance
    2. 6.2 Failure Information Collection and Analysis Guidance
  10. Common Development Questions
    1. 7.1 Unlock MCU
      1. 7.1.1 Unlock Through Bootloader
      2. 7.1.2 Unlock Through Factory Reset GUI Tool
      3. 7.1.3 Unlock Through Uniflash
      4. 7.1.4 Unlock Through CCS
      5. 7.1.5 Unlock With Reset Pin Disabled
    2. 7.2 MSPM0 Program Failure
    3. 7.3 Attentions When Disabling SWD or REST Pin
    4. 7.4 MCU Performs Differently in Debug and Free Run
    5. 7.5 Set SWD Password
    6. 7.6 BSL Related Questions
    7. 7.7 Reach Expected Current in LPM Mode
    8. 7.8 CCS Common Questions
      1. 7.8.1 Change the Optimization Level
    9. 7.9 Keil Common Questions
      1. 7.9.1 Copy Keil Example Out of SDK
  11. Summary
  12. Technical Documentation Resources
    1. 9.1 Technical Reference Manuals
    2. 9.2 Subsystems
    3. 9.3 Reference Designs
    4. 9.4 Hardware EVM User's Guides
    5. 9.5 Application Briefs
    6. 9.6 Application Notes and Others
  13. 10Revision History

Attentions When Disabling SWD or REST Pin

There are three attentions that users need to know before disabling SWD or REST pin.

  • Attention 1: After the SWD or REST pin is disabled, they can only be re-enabled by a POR. Normally a re-power is suggested. It also means it is impossible to re-enable through software in free run mode.
  • Attention 2: SWDIO and SWCLK have default pullup and pulldown resistors. Users need to disable them by controlling IOMUX register though sysconfig or C code directly, especially when these two pins are used as input or analog functions.
  • Attention 3: Disabling SWD makes it hard for reprogramming. Here are the common methods:
    • Add a delay like 5 seconds before SYSCFG_DL_init(). With that, users have some time to connect MSPM0 before disabling SWD is executed.
    • Use ROM Bootloader. Before powering on MSPM0, pull and hold PA18 to be high. Program the flash with the right code. Then release PA18.
    • Use factory reset. Before powering on, press and hold the reset button. Perform a factory reset according to Section 7.1. When prompted to reset the chip, release the reset button. Then, the chip is blank.