SLAU131Y October 2004 – June 2021
Set Listing Page Size
.length [page length]
.width [page width]
Two directives allow you to control the size of the output listing file.
The .length directive sets the page length of the output listing file. It affects the current and following pages. You can reset the page length with another .length directive.
The .width directive sets the page width of the output listing file. It affects the next line assembled and the lines following. You can reset the page width with another .width directive.
The width refers to a full line in a listing file; the line counter value, SPC value, and object code are counted as part of the width of a line. Comments and other portions of a source statement that extend beyond the page width are truncated in the listing.
The assembler does not list the .width and .length directives.
The following example shows how to change the page length and width.
********************************************
** Page length = 65 lines **
** Page width = 85 characters **
********************************************
.length 65
.width 85
********************************************
** Page length = 55 lines **
** Page width = 100 characters **
********************************************
.length 55
.width 100