SLAU131Y October 2004 – June 2021
In this example, three tasks exist in separate load areas. As each is needed, it is copied into the common run area and executed. A separate copy table is generated for each task (see table() operator in ex1.cmd). CRC values for the task functions are verified as well. See Section C.3.6 for the crc_table() operator calls.
To run a simple example that uses copy tables and CRC tables, follow these steps: