SLAU833A May   2020  – October 2020 ADC12DJ3200

 

  1.   1
  2.   2
  3.   3
  4.   4
    1.     5
    2.     6
    3.     7
  5.   8
    1.     9
      1.      10
    2.     11
  6.   12
  7.   13
    1.     14
    2.     15
      1.      16
    3.     17
  8.   18

Programming the FPGA

This section provides instructions for programming the FPGA.

Launch Vivado 2019.1 and open the Hardware Manager.

GUID-0DB2CF86-91EC-45D0-A0D7-F4576F798BBC-low.pngFigure 7-6 Vivado® Main Menu

Select “Open Target”.

GUID-4A9AC12D-3E0A-4F9B-920C-A744B9C0457B-low.pngFigure 7-7 Open Target

Select “Auto Connect”

GUID-75A72802-D9C0-411D-9CA3-2D70D9681E00-low.pngFigure 7-8 Auto Connect

Right click on the xcku060… device and select “Program”.

GUID-2F24F29D-A0DB-4BDB-85DF-E2E25CA35B03-low.pngFigure 7-9 Select Device

Navigate to C:\AlphaData_ADC12DJ3200_Demo and select the file “alpha-data-samples.bit”.

GUID-39CF37DA-909C-4460-B725-95D7AB5F5EDD-low.pngFigure 7-10 Navigate to bit File Location

Click the Program button to complete the FPGA configuration with the bitfile.

GUID-B925BB45-5DF7-40FF-B7ED-597B99CC10CA-low.pngFigure 7-11 Program Device With the bit File

In the Vivado TCL console, execute the following:

  • cd c:/AlphaData_ADC12DJ3200_Demo
  • source setup_new.txt

Switch back to the ADC12DJ3200EVM-CVAL GUI.

Navigate to the JESD204B tab and click on the JSYNC_N Sync Request button (it should now be off, as Figure 7-12 shows).

Switch back to the Vivado setup.

In the Vivado TCL console, execute the following:

cd c:/AlphaData_ADC12DJ3200_Demo

source capture_new.txt

The FPGA will now be doing continuous captures of the ADC data.

GUID-D2D9F202-CBE3-4650-BC17-9440531E885C-low.pngFigure 7-12 Send SYNC High to ADC