SLUUDI6 December 2025 MSPM33C321A
Memory Address: 0x80101C3C
The I2C_SLAVE_ADDR field specifies the slave address used by the BSL when operating in I2C mode. External devices must use this address to communicate with the BSL over the I2C interface.
Bits: 15...0
Default Value: 0x48
The I2C_SLAVE_ADDR field sets the slave address that the BSL uses when communicating over the I2C interface. When the BSL is invoked and the I2C interface is selected, it configures the I2C peripheral to respond to this slave address.