SLUUDI6 December 2025 MSPM33C321A
The READOUT field controls whether the BSL allows memory readout operations. When enabled, the Memory Read Back command can be used to read the contents of flash and SRAM memory. When disabled, the Memory Read Back command will return an error.
Default Value: BL_CFG_READBACK_EN (0xAABB)
Valid Values:
By default, memory readout is disabled for security reasons. It should only be enabled in developing environments or when memory readout is specifically required.
Even when memory readout is enabled, the BSL must still be unlocked with the correct password before the Memory Read Back command can be used. This provides an additional layer of security to prevent unauthorized access to the memory contents.