SLUUDI6 December 2025 MSPM33C321A
The data packets of the UART and I2C BSL protocol have the following structure.
| PI Code | BSL Core Data | PI Code | |
|---|---|---|---|
| Header (1 byte) | Length (2 byte) | BSL Core Command/Response | CRC32 (4 byte) |
Based on the Core data field, the data packet is classified as either Command packet or response packet.
Command packet is the first packet which is transmitted to the BSL. The second packet is the Response packet which is received from the BSL. Response packet contains two components BSL acknowledgment and BSL Core response. In these two, Acknowledgment is received from BSL for every command packet sent. But the BSL core response is not received for every command.
Figure 3-1 BSL Protocol