SLVSA00E September 2009 – April 2015
PRODUCTION DATA.
Three evaluation modules (EVMs) are available to assist in the initial circuit performance evaluation using the TLV700:
These EVMs can be requested at the Texas Instruments website through the product folders or purchased directly from the TI eStore.
Computer simulation of circuit performance using SPICE is often useful when analyzing the performance of analog circuits and systems. A SPICE model for the TLV700 is available through the product folders under Tools & Software.
| PRODUCT | VOUT(2) |
|---|---|
| TLV700xxyyyz | XX is nominal output voltage (for example, 28 = 2.8 V). YYY is the package designator. Z is tape and reel quantity (R = 3000, T = 250). |
Bluetooth is a registered trademark of Bluetooth SIG.
All other trademarks are the property of their respective owners.
ZigBee is a registered trademark of the ZigBee Alliance.

These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.