Use the following instructions to perform the
overcurrent test on the current limit TPS25948 eFuse on channel 1:
- Place jumper J8 to the appropriate position to obtain required blanking period
as per Table 4-3.
- Set the input supply voltage VIN to 12 V and current limit of 9 A and enable the power supply.
- Place jumper J6 in good position to set the required current limit as per Table 4-3.
- Apply an overload greater than the set current limit between VOUT1 and GND.
- The device allows the overload current for the programmed ITIMER period and then starts limiting current.
Figure 5-3 shows an example of the circuit breaker test on the TPS25948EVM.