SLWU087E november 2013 – june 2023
The FPGA Registers Write Read menu option (shown in Figure 3-8) allows the user to write/read the registers of the FPGA Firmware. The firmware register map of the TSW14xxx board is loaded and the Register Name, Register Address, R/W Mode, Register Values and Register Description is shown. The register write operation is done by selecting the required register element from the tree or by specifying the required register address in the "Address" input control and providing a value to be written at "Write Data" input control and then clicking on the "Write Register" button. Similarly, the register read operation is done by clicking on the "Read Register" button after specifying the required register address and the read register value are updated both in the register tree and "Read Data" output indicator. The current register configuration listed in the register map is exported as “.cfg” file by using the “Save Config” button and the same is loaded by using the “Load Config” button. The “Load Config” operation overwrites the existing data in registers with the value specified in the loaded configuration file.