SNAA378 January   2023 LMX1204

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Test Setup
  5. 3Measurement Results
    1. 3.1 Input/Output Return Loss
    2. 3.2 Group Delay
    3. 3.3 Phase Error Within One LMX1204 Device
    4. 3.4 Phase Error Across all LMX1204 Channels
  6. 4Conclusion
  7. 5References

Phase Error Within One LMX1204 Device

Figure 3-3 shows the phase error relative to the average phase within one LMX1204 device across the 4 channels. Within a single device, the phase response is very consistent across each of the channels. Based on information from the LMX1204 data sheet, the expected skew between channels in one device is less than 2 ps. In this case, there is variation within the device in addition to tolerance variations within the output traces and RF cables.

GUID-20221207-SS0I-KWNS-WHHP-H2MLQX3FHKMG-low.png Figure 3-3 Phase Error Across Channels of one LMX1204 Device