SNLU223D August 2017 – February 2023 DS90UB954-Q1
Register settings can be saved and later loaded to the device using the "Save" and "Load" buttons. To save, click on the "Save" button, select the file location, and name the file. If desired, comments may be recorded about the register settings . After the registers are saved, a dialog box will appear confirming that the registers were saved successfully. To load saved registers, click the "Load" button and select the .nrd file. Additional information about the register settings, including any comments, will be displayed in the dialog box. After confirming these are the desired registers settings, a message will appear confirming that the registers were successfully loaded.