SNOAA91 may 2023 TLV1812 , TLV1851 , TLV7011
If the Absolute Maximum Ratings upper input voltage is referenced to the supply, such as "V+" or "Vcc + 0.2", then that is a good sign that there is an upper ESD clamp. Excursions outside the supplies need to be limited to prevent the ESD diodes from conducting (typically around 500 mV - 600 mV depending on process).
Figure 3-2 from the TLV1812 data sheet Absolute Maximum Ratings table shows an example of the ESD clamped inputs. Notice that the highlighted "Input Pins" row shows a Max of "(V+) + 0.3", which is referred to the V+ power supply rail.