SNOU181B February 2021 – April 2022
The BOOST-LDC3114EVM includes four identical example sensors that are perforated so they can be removed and replaced with different sensors by soldering onto the provided header pin locations. The LDCCOILEVM and LDCTOUCHCOMCOILEVM both have compatible sensors that can be used with the BOOST-LDC3114EVM and can be obtained if testing with various sensor designs is necessary. Other sensors can be connected to the input headers with an unshielded twisted pair of wires. The included sensors are designed to allow the 3D printed attachments that come with the EVM to attach to the board.