SNOU181B February 2021 – April 2022 LDC3114 , LDC3114-Q1
Figure 1-2 shows the layout of the BOOST-LDC3114EVM and points out various features. The sensor coils are located on a perforated section of the board so they can be placed remotely from the sensor or replaced with other, compatible sensors by using the sensor connection headers.
The BOOST-LDC3114EVM has multiple test points designated for the power, ground, I2C, and output pins. Additionally, the button detection LEDs on the output pins are located in the center of the board. The test points connected to the sensors have a resistor pad that can be populated with a 1-kΩ resistor to decouple the oscilloscope probe capacitance.
Figure 1-2 EVM Features.