SNVU651 January 2019
To show or hide the console, toggle the option in the View pulldown menu. The console can be used to access any of the TPS65653 registers. Registers can be read or written simply by referring to the logical registers by their name.
The console supports use of scripts. If a text file containing commands supported by the console is stored in the same folder as the evaluation software executable, then the script can be launched from the console by typing the text file name, like script.txt.