SPRACU8B August 2021 – January 2023 AM68 , AM68 , AM68A , AM68A , AM69 , AM69 , AM69A , AM69A , DRA821U , DRA821U , DRA829V , DRA829V , TDA4VM , TDA4VM
The four user output worksheets include:
Each output worksheet contains the calculated register settings in the corresponding software repository format. As an example, the RTOS worksheet provides the register settings in an array format utilized by the secondary bootloader (SBL) DDR driver, while the u-boot worksheet provides the register settings as a #define preprocessor directive. In addition, each worksheet contains a "Save" left-click push button to allow the contents of the worksheet to be saved to your hard drive. Figure 1-2 shows an example of a "Save" left-click push button.
Figure 1-2 "Save" Left-Click Push
Button