SPRAD09A December 2021 – July 2022 DRA821U , DRA821U-Q1
This is the cold boot until the Kernel login, the cost time is about ~3 seconds.
From the log result in the following picture, we have (10.070 – 7.098) = 2.972 seconds.
Comparing the original Linux boot (2X~4X seconds), this fast boot result is good enough for automotive applications.
User can base on this to do those following developing:
Figure 5-1 Jacinto DRA821U Fast Boot
Result