SPRAD61A March 2023 – November 2023 AM2732 , AM2732 , AM2732-Q1 , AM2732-Q1
On the AM273 NZN Four Layer Example, the 3.3 V plane is shown routing to and underneath the AM273 device primarily on layer 3. Due to routing limitations caused by a four layer PCB, underneath the AM273 device the 3.3 V plane is split between layer 2 and layer 3.
The 3.3 V plane on layer 2 break up the otherwise solid ground pour on layer 2. The placement of the cutout was chosen to minimize the impact to the signal return paths for as many GPIO pins as possible. Vias connect the planes on layers 2 and 3 to the BGA ball pads on the top layer and the decoupling capacitors on the bottom layer.
Figure 11-19 NZN 4 Layer Example Excerpt – 3.3 V Digital and Analog Power Planes on Layers 2 and 3 and BGA Vias
Figure 11-20 NZN 4 Layer Example Excerpt – 3.3 V Decoupling