SPRAD86 March 2023 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM68A , AM69A
After raw images are captured, start the AWB tuning from the "Plug-ins" drop down menu. Import the raw images one by one in the “Reference files” tab (see the AWB plugin guide for details) and enter the parameter values for each image:
Please pay special attention when selecting the corners of the color checker chart:
#GUID-EE3717A6-649F-4999-84B2-213465839603 through #FIG_HFZ_DVC_RWB show an example of importing one raw image for AWB tuning.
After importing all raw images, follow the AWB plugin guide to do the tuning. If tuning is successful, reference Cb-Cr plot scheme will be displayed. Below is the result plot using the raw images shown above.
After tuning is done, generate new output XML files and new binary files as done in tuning Black Level Subtraction. Then use the newly generated DCC binary files to stream and capture. #FIG_GVT_KVC_RWB and #FIG_RZ4_PVC_RWB show images captured before AWB tuning and after AWB tuning (all gray patches appear neutral in the image after AWB tuning).