Locate the PHY addresses of the
add-on board with an MDIO scan or check the corresponding registers in the
MDIO-PHY interface.
Change the PHY addresses in the
SysConfig-GUI for instances of ICSSG0 in the Board Config section to the PHY
address locations found on the specific board.
Build the following example in
the test folder: make -s -C
test/networking/lwip/enet_icssg_tcpserver/am64x-evm/r5fss0-0_freertos/ti-arm-clang
clean all