SPRADH8 September   2024 AM6442

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
    1. 1.1 AM64x and AM243x EVMs
    2. 1.2 SoC Architecture
      1. 1.2.1 AM64x
      2. 1.2.2 AM243x
    3. 1.3 Peripherals
      1. 1.3.1 CPSW3G
      2. 1.3.2 PRU-ICSSG
    4. 1.4 Ethernet Software Architecture
    5. 1.5 Prerequisite
      1. 1.5.1 HW Prerequisite
      2. 1.5.2 SW Prerequisite
        1. 1.5.2.1 Resource Allocation - AM64x
        2. 1.5.2.2 SBL update
  5. Multicore 5-Ethernet Ports Realization
  6. Supported Configurations on PRU-ICSSG
  7. Implementation
    1. 4.1 System Example
      1. 4.1.1 Software Architecture
      2. 4.1.2 5-Ethernet Port Example
  8. Debug Steps
  9. Reference Logs
  10. Testing for the ICSSG0 and ICSSG1 Functionality
  11. ICSSG and CPSW
  12. Summary
  13. 10References

Multicore 5-Ethernet Ports Realization

Multicore 5-Ethernet ports can be realized by one of the two methods shown below:

  • 2-Ethernet ports from ICSSG0, 2-Ethernet ports from ICSSG1, and 1-Ethernet port from CPSW.

or

  • 2-Ethernet ports from ICSSG0, 1-Ethernet port from ICSSG1, and 2-Ethernet ports from CPSW.

These are the details on the method that can be realized using a SEM extension card with an HSE port, which adds two additional Ethernet ports for ICSSG0.