This section presents some important
considerations when selecting crystals for the CC31xx and CC32xx. Selecting a crystal
for a specific application will depend on the following three factors:
- Size (footprint area and height)
- Performance (accuracy over
temperature, lifetime, power consumption, and start-up time)
- Cost
Consider the following when selecting a
crystal:
- Crystals must be selected to meet
requirements listed in the CC31xx and CC32xx data sheets or specifications.
- ESR must not be greater than
can be driven by CC31xx and CC32xx.
- Capacitive loading
(CL) and frequency tolerance (ppm) must meet the
specifications of the standard used (for example, Wi-Fi®).
- Some other considerations when
selecting a crystal include the following:
- To improve start-up time and
reduce power consumption, the crystal must have the following:
- Low-capacitive
loading, at the expense of greater susceptibility to frequency
variation caused by the environment (CL)
- Low-motional
inductance (LM)
- Low-motional
resistance (RM)