SWRA772 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Running the Bluetooth Code
  6. Demo Application
    1. 3.1 Device 1 (Server) Setup on the Demo Application
    2. 3.2 Device 2 (Client) Setup on the Demo Application
    3. 3.3 Initiating Connection from Device 2
    4. 3.4 Identify Supported Services
    5. 3.5 Data Transfer Between Client and Server
    6. 3.6 Multiple SPPLE Connections Guide
  7. Demonstrating SPP LE on an iOS Device with the LightBlue App
    1. 4.1 LightBlue Overview
    2. 4.2 SPP LE Service Overview
      1. 4.2.1 Characteristics
  8. LightBlue as the Client/SPPLEDemo as the Server
    1. 5.1 Connecting the Devices
    2. 5.2 Enabling Notifications
    3. 5.3 Sending Data from LightBlue/Receiving Data in SPPLEDemo
    4. 5.4 Sending Data from SPPLEDemo/Receiving Data in LightBlue
  9. LightBlue as the Server/SPPLEDemo as the Client
    1. 6.1 Connecting the Devices
    2. 6.2 Sending Data from LightBlue/Receiving Data in SPPLEDemo
    3. 6.3 Sending Data from SPPLEDemo/Receiving Data in LightBlue
  10. Application Commands
  11. General Commands
    1. 8.1 Help (DisplayHelp)
    2. 8.2 Get Local Address
    3. 8.3 Set Baud Rate
    4. 8.4 Quit
  12. BR/EDR Commands
  13. 10GAPLE Commands
    1. 10.1  Set Discoverability Mode
    2. 10.2  Set Connectability Mode
    3. 10.3  Set Pairability Mode
    4. 10.4  Change Pairing Parameters
    5. 10.5  Advertise LE
    6. 10.6  Start Scanning
    7. 10.7  Stop Scanning
    8. 10.8  Connect LE
    9. 10.9  Disconnect LE
    10. 10.10 Pair LE
    11. 10.11 LE Pass Key Response
    12. 10.12 LE Query Encryption
    13. 10.13 Set Passkey
    14. 10.14 Discover GAPS
    15. 10.15 Get Local Name
    16. 10.16 Set Local Name
    17. 10.17 Get Remote Name
    18. 10.18 LE User Confirmation Response
    19. 10.19 Enable SC Only
    20. 10.20 Regenerate P256 Local Keys
    21. 10.21 SC Generate OOB Local Params
    22. 10.22 Set Local Appearance
    23. 10.23 Get Local Appearance
  14. 11SPPLE Commands
    1. 11.1 Discover SPPLE
    2. 11.2 Register SPPLE
    3. 11.3 LE Send
    4. 11.4 Configure SPPLE
    5. 11.5 LE Read
    6. 11.6 Loopback
    7. 11.7 Display Raw Mode Data
    8. 11.8 Automatic Read Mode
  15. 12References
  16. 13Revision History

Regenerate P256 Local Keys

Description

The following function allows the user to generate new P256 private and local keys. This function shall NOT be used in the middle of a pairing process. This is relevant for LE SecureConenctions pairing only. This function returns zero on successful execution and a negative value on all errors.

Parameters

No parameters are necessary.

Command Call Examples

“RegenerateP256LocalKeys” Attempts to generate new P256 private and local keys.

Possible Return Values

  • (0) Success.
  • (-4) FUNCTION_ERROR.
  • (-8) INVALID_STACK_ID_ERROR.
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.
  • (-56) BTPS_ERROR_GAP_NOT_INITIALIZED.
  • (-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.
  • (-117) BTPS_ERROR_PAIRING_ACTIVE.
  • (-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call

GAP_LE_SC_Regenerate_P256_Local_Keys (BluetoothStackID)

API Prototype

int BTPSAPI GAP_LE_SC_Regenerate_P256_Local_Keys (unsigned int BluetoothStackID)

Description of API

The following function is provided to allow a regeneration of the P-256 private and local puclic keys. This function is relevant only in case of LE SC pairing. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device. This functions shall NOT be used while performing pairing. This function returns zero if successful or a negative error code.