On the separate LaunchPad:
- Remove all of the header jumpers
except GND and 3V3.
- Set the power jumper to reflect
the scenario. Set the jumper to XDS110 power if the LP-EM-CC2745R10-Q1 is to be powered by the separate
LaunchPad. Set this to Extern Pwr if external power is to be provided
instead. Care must be taken to keep the board voltage within the board's
operating range (1.8V to 3.6V).
- Connect one end of the 10-pin
Debug Cable to the XDS110 Out connector on the LaunchPad.
- Connect one end of the 2-wire
Power Cable to the 3V3 and GND header of the LaunchPad.
On the (LP-EM-CC2745R10-Q1):
- Connect the other end of the
10-pin Debug Cable to the Target In connector.
- Connect the other end of the
2-wire Power Cable to the GND and 3V3 header. Verify that the
polarity is correct.
The final configuration is shown
in Figure 2-3.