TIDA029A july 2019 – june 2023 CC2640R2F-Q1 , CC2642R , CC2642R-Q1
The following sections show various test results based off the TIDA-01632 antenna design. All test results were taken in an anechoic chamber using the turntable shown in Figure 3-13, capable of rotating the base and the arm by 1° increments.
Figure 3-13 Turntable Test SetupFigure 3-14 shows the TIDA-01632 PCB mounted on the arm of the turntable and Figure 3-15 shows the rest of the anechoic chamber.
Figure 3-14 PCB Mounted on Turntable Arm
Figure 3-15 Anechoic Chamber