DLPU062B March 2018 – January 2024 DLPC3437
Table 3-115 describes the write parameters.
| MSB | Byte 1 | LSB | |||||
|---|---|---|---|---|---|---|---|
| b7 | b6 | b5 | b4 | b3 | b2 | b1 | b0 |
| b(7:3) | Reserved |
| b(2:0) | Display border color:
|
Whenever the display image size is smaller than the active area of the DMD, the border color is used for all non-image pixels. Some examples using a border include a window box, pillar box, or letterbox image.
To display a pillar box image (see Figure 3-18), the user can use the border color defined by this command.
The border color specified by this command is separate from the curtain color defined in the Display Image Curtain command, though both display using the curtain capability.
Whenever the keystone capability is used, the user should set the border color to black. Setting this parameter to any other color when keystone is enabled produces undesirable results.
Figure 3-18 Pillar-Box Border Example