DLPU102D December   2020  – October 2025

 

  1.   1
  2.   Read This First
    1.     About This Guide
    2.     Related Documentation from Texas Instruments
    3.     If You Need Assistance
  3.   Trademarks
  4.   7
  5. 1DLP LightCrafter Dual DLPC900 EVM Overview
    1. 1.1 Welcome
    2. 1.2 DLP LightCrafter Dual DLPC900 Evaluation Module (EVM) Hardware
    3. 1.3 EVM Board
    4. 1.4 Other Items Needed for Operation
    5. 1.5 DLP LightCrafter Dual DLPC900 Connections
      1. 1.5.1 DLP LightCrafter Dual DLPC900 LED Enable and PWM Outputs
      2. 1.5.2 DLP LightCrafter Dual DLPC900 Trigger Input and Output Voltage Selectors
    6. 1.6 DLP LightCrafter Dual DLPC900 EVM Flex Cable
    7. 1.7 DLP LightCrafter Dual DLPC900 EVM and DMD EVM Assembly
  6. 2Quick Start
    1. 2.1 Power-up the DLP LightCrafter Dual DLPC900 EVM
    2. 2.2 Creating A Simple Pattern Sequence
  7. 3Operating the DLP LightCrafter Dual DLPC900 EVM
    1. 3.1  DLP LightCrafter Dual DLPC900 Control Software
    2. 3.2  PC Software
    3. 3.3  System Common Controls
      1. 3.3.1 Operating Mode
      2. 3.3.2 Connected DMD Type
      3. 3.3.3 EVM Information
      4. 3.3.4 Status
    4. 3.4  System Settings
    5. 3.5  Video Mode
      1. 3.5.1 Video Support
    6. 3.6  Pattern Modes
      1. 3.6.1 Menu Bar
      2. 3.6.2 Creating a Pattern Sequence in Pattern On-The-Fly Mode
      3. 3.6.3 Creating a Pattern Sequence in Pre-Stored Pattern Mode
      4. 3.6.4 Reordering a Pattern Sequence using the Edit LUT Feature
        1. 3.6.4.1 Special Considerations for Input Triggers When Using the Edit LUT Feature
      5. 3.6.5 Creating a Pattern Sequence in Video Pattern Mode
      6. 3.6.6 Creating a Pattern Sequence With DMD Block Load
      7. 3.6.7 Pattern Settings
    7. 3.7  Batch Files
      1. 3.7.1 Execute Batch File
      2. 3.7.2 Creating and Saving Batch Files
        1. 3.7.2.1 Creating and Saving a Batch File Using the GUI
        2. 3.7.2.2 Creating a Batch File Using a Text Editor
      3. 3.7.3 Loading a Batch File
      4. 3.7.4 Adding a Batch File to the Firmware
    8. 3.8  Peripherals Panel
      1. 3.8.1 Peripherals Tab
      2. 3.8.2 Debug Tab
    9. 3.9  Firmware
      1. 3.9.1 Adding or Removing Patterns from the Firmware
        1. 3.9.1.1 Deleting Images
        2. 3.9.1.2 Adding Images
        3. 3.9.1.3 Adding Both Images and Batch Files
    10. 3.10 Reprogram Controller Board for a Different Supported DMD
    11. 3.11 Flash Device Parameters
    12. 3.12 JTAG Flash Programming
    13. 3.13 Programming an EDID
    14. 3.14 Intel (Altera) FPGA Programming
  8. 4Connectors
    1. 4.1  Input Trigger Connectors
    2. 4.2  Output Trigger Connectors
    3. 4.3  DLPC900 UART Headers
    4. 4.4  DLPC900 I2C Port 0
    5. 4.5  DLPC900 I2C Port 1
    6. 4.6  DLPC900 I2C Port 2
    7. 4.7  JTAG Boundary Scan
    8. 4.8  GPIO and PWM
    9. 4.9  Power
    10. 4.10 External Parallel Video Connector
  9. 5Power Supply Requirements
    1. 5.1 External Power Supply Requirements
  10. 6Safety
    1. 6.1 Caution Labels
  11. 7Revision History

Creating a Pattern Sequence in Pattern On-The-Fly Mode

Pattern On-The-Fly Mode is the easiest and quickest way to create a pattern sequence. Follow these steps to create a simple pattern sequence using three images

  1. Make sure the EVM is powered up and operating correctly, and the Connected radio button is lit green.
  2. Select Pattern On-The-Fly Mode from the Operating Mode group box, and then click the Pattern Design button so that the large black panel is displayed as shown in Figure 3-6.
  3. Click the Add Pattern button in the Menu bar and browse for any three bitmap images from the sample of images directory. Be sure to select them from the correct image folder for the EVM that is being used. All three images can be selected at the same time within the open file dialog window. When selecting multiple files at once, the operating system does not load the images in the same order as selected. To add images in a predefined order, use the Load button. This option loads the images from a text file that contains the file names of each bitmap in the desired order. Alternatively, you can add the images one at a time using the Add Pattern button to verify the order. Figure 3-8 shows an example of loading images from a file. The bitmap images must be located in the same directory as the text file. See Figure 3-9 after the images have been added.
    DLPC900 Add From ListFigure 3-8 Add From List
    DLPC900 Pattern SequenceFigure 3-9 Pattern Sequence
  4. Each pattern in the display can now be selected individually or a multiple selection can be done. To select multiple patterns in a series, use Shift+Click. To select multiple patterns that are not in a series, use Ctrl+Click. An alternate method for selecting all images is to use the Select All Patterns button on the Menu bar.
  5. Select the first pattern and choose a bit depth of 1. Set exposure to 100000µs and set dark time to 50000µs. The dark time is the time from the end of one pattern to the start of the next pattern. Select Red for the color.
  6. Select the second pattern and choose a bit depth of 1. Set exposure to 150000µs and set dark time to 75000µs, and select Green as the color.
  7. Select the third pattern and choose a bit depth of 1. Set exposure to 200000µs and set dark time to 100000µs, and select Blue as the color. Figure 3-10 shows the pattern sequence. The Zoom bar can be used to zoom in and out which is useful when many patterns are loaded into the panel.
    DLPC900 Three Pattern SequenceFigure 3-10 Three Pattern Sequence
  8. Select the Repeat radio button to continuously repeat the pattern sequence, or, if only one time is desired, then select the Play Once radio button.
  9. Click the Update LUT button to upload the pattern sequence definition, including the three pattern images, to the DLPC900. Notice the green status bar indicating that the updated LUT is uploading to the EVM. This animation does not occur if the user only edits pattern settings rather than uploading actual new patterns. If there are any errors in the pattern sequence, the GUI displays an error message.
  10. Once the upload is complete, click the Start button. The display repeatedly displays the Red, Green, and Blue dots.
  11. To pause the pattern sequence, click the Pause button. To continue from where the pattern sequence paused, click the Start button.
  12. To stop the pattern sequence, click the Stop button. To restart the pattern sequence, click the Start button. The pattern sequence starts from the beginning whenever the pattern sequence is stopped using the Stop button.

Another method of creating a pattern sequence in Patten On-The-Fly Mode is using a batch file that contains all the necessary commands and the compressed images.

Follow these steps to execute a pattern sequence using a batch file.

  1. Stop the pattern sequence if currently running.
  2. Click the Batch Files button at the top of the GUI.
  3. Check the box to Enable Command Logging.
  4. Click the Clear All button to clear any content in the panel.
  5. Click the Load Batch File button and select the onthefly.txt file located in the sample images directory. Be sure to select the correct file for the EVM being used.
  6. Click the Execute All button. Wait for the batch file to execute.
  7. Click the Pattern Mode button at the top of the GUI.
  8. Click the Start button.
  9. Click the Stop button to end this example.