DLPU133B March 2024 – August 2026 DLPC964
Aurora is a generic data transport link without concept of a DMD block. To define the start of a DMD block, the Apps user logics must send a Block Control word packet through channel 0 Aurora user-k port before data transmission.
Refer to Xilinx app note Chapter 2 Table 2-10 for detailed information regarding the Aurora user-k interface port. In summary, the user-k interface ports are used to implement application-specific control functions, and are independent and higher priority than the data interface. As shown in Table 8-2, the RTL wrapper aurora_apps_tx_x12ln.v has four channels of user-k port interface exposed to Apps FPGA user logics.
| Signal Name | Signal Direction | DLPC964 Application Usage |
|---|---|---|
| gt0_s_axi_user_k_tx_tdata[191:0] | Input to Aurora Channel 0 | 192 bits Block Control word packet to be transmitted |
| gt0_s_axi_user_k_tx_tvalid | Input to Aurora Channel 0 |
User logics asserted this signal high to indicate to Aurora core the Block Control word is valid to transmit. Aurora cores ignore word if tvalid is low. |
| gt0_s_axi_user_k_tx_tready | Output from Aurora Channel 0 |
Aurora cores assert this signal high when the Block Control word is accepted. Deasserted when words are ignored, that is, cores are not ready to accept input word. |
| gt1_s_axi_user_k_tx_tdata[191:0] | Input to Aurora Channel 1 | Unused |
| gt1_s_axi_user_k_tx_tvalid | Input to Aurora Channel 1 | Unused |
| gt1_s_axi_user_k_tx_tready | Output from Aurora Channel 1 | Unused |
| gt2_s_axi_user_k_tx_tdata[191:0] | Input to Aurora Channel 2 | Unused |
| gt2_s_axi_user_k_tx_tvalid | Input to Aurora Channel 2 | Unused |
| gt2_s_axi_user_k_tx_tready | Output from Aurora Channel 2 | Unused |
| gt3_s_axi_user_k_tx_tdata[191:0] | Input to Aurora Channel 3 | Unused |
| gt3_s_axi_user_k_tx_tvalid | Input to Aurora Channel 3 | Unused |
| gt3_s_axi_user_k_tx_tready | Output from Aurora Channel 3 | Unused |
Table 8-3 describes the various fields within the 192 bits Block Control word. Block Control word not only defines the start of a DMD block, but also contains instruction and information to guide the DLPC964 controller on how to process the receiving DMD block data
| Field Position | Field Type | Field Description |
|---|---|---|
| gt0_s_axi_user_k_tx_tdata[7:0] | USER_BLOCK_NUMBER | Must set to zeros (0x00). Values other than 0x00 are invalid, DLPC964 controller ignores the entire 192 bits control word if this field is not zeros. |
| gt0_s_axi_user_k_tx_tdata[11:8] | BLOCK_ADDRESS |
Indicates the address of the DMD block to which DLPC964 applies the operation. 0000: DMD Block 0 0001: DMD Block 1, 0010: DMD Block 2 ….…. 1111: DMD Block 15 |
| gt0_s_axi_user_k_tx_tdata[15:7] | Reserved, unused. | |
| gt0_s_axi_user_k_tx_tdata[24:16] | ROW_LENGTH | Number of row DLPC964 loads the user
data. DLP991U and DLP991UUV DMD has 136 rows per block, thus valid
range is 1-136. All other values, including 0 are invalid. Set to
136 for full block operation. Value 1 to 135 for partial block.
Note: This field used if LOAD_TYPE is
000. |
| gt0_s_axi_user_k_tx_tdata[34:32] | LOAD_TYPE |
000: Block loading. DLPC964 load the user data to the DMD array area defined by the BLOCK_ADDRESS and ROW_LENGTH. 001: Block clear. DLPC964 clear the DMD array to zeros of the entire block define by BLOCK_ADDRESS. 010: Block set. DLPC964 set the DMD array to ones of the entire block defined by BLOCK_ADDRESS. Other values: reserved, do not use. Note: When in 001 (block clear) or 010 (block
set) operation, the ROW_LENGTHand NORTH_SOUTH_FLIP fields are
ignored because clear and set operation affect the entire DMD
block array. In other words, block set/clear operation do not
support partial block operation.
|
| gt0_s_axi_user_k_tx_tdata[36] | NORTH_SOUTH_FLIP |
Control the direction of data loading within a DMD block. 0: DLPC964 load data starting and counting up from row 1. 1: DLPC964 load data starting and counting down from row 136. |
| gt0_s_axi_user_k_tx_tdata[29:28] | DMD_SEGMENT |
When SINGLE_CHANNEL_MODE = '1', select the DMD segment to which the DLC964 applies the operation. DLPC964 Controller ignores this field if SINGLE_CHANNEL_MODE = '0'. |
| gt0_s_axi_user_k_tx_tdata[30] | SINGLE_CHANNEL_MODE |
1: Single channel operation. Operate the DMD array with only Aurora channel 0. 0: Normal operation. Operate the DMD array with all four Aurora channels. |
| gt0_s_axi_user_k_tx_tdata[191:31] | reserved, unused. |
Figure 8-17 shows the transmission of the 192 bits Block Control word over the channel 0 user-k port at the start of an Aurora block transfer (in this example, loading all 136 lines of DMD block 1).
Figure 8-17 Block Start with Block Control
Word Waveform