SBAA188B July 2011 – October 2026 ADS1191 , ADS1192 , ADS1194 , ADS1196 , ADS1198 , ADS1291 , ADS1292 , ADS1292R , ADS1294 , ADS1294R , ADS1296 , ADS1296R , ADS1298 , ADS1298R , ADS1299
Common-mode rejection, or CMR, is one of the most important performance parameters for ECG system applications. International standards set by organizations such as the Association for the Advancement of Medical Instrumentation (AAMI), the International Electrotechnical Commission (IEC), and various medical authorities of different countries specify the test methodology that must be followed in order to use most ECG systems.
In an ECG system, a large amount of electromagnetic interference (EMI) is coupled to the patient’s body through the skin. EMI can also couple to the ECG system through coupling capacitors C2 and CT as shown in Figure 1-1. Furthermore, It can be coupled to the system through a power coupling capacitor, CC, and in some cases through the long ECG signal measuring cables and protection circuitry that are usually located in front of the ECG system. There can also be coupling from the ac power supplies through coupling capacitor CCB to the cable. Capacitance CB is coupled between ac ground and the ground of the ECG subsystem. The value of the entire system CMR depends on the capacitance value of CB. By comparison, in the case of a perfectly isolated system where there is no coupling between the grounds, the system would exhibit very high CMR.
There are also several frequencies of interest, depending on the location and the country of operation. The primary source of interference is the ac main that generally operates at 50 Hz (Europe and Asia) or 60 Hz (US). Apart from these two frequencies, Eastern European railway traction power networks use distributed single‐phase ac power at 16⅔ Hz. A frequency of 25 Hz is used for the Austrian railway.
Figure 1-1 Typical ECG System