SBAA277B February 2018 – September 2024 ADS8860 , INA826 , OPA192
| Input | ADC Input | Digital Output ADS8860 |
|---|---|---|
| –10mV | Out = 0.2V | 0A3DH or 262110 |
| 5mV | Out = 4.8V | F5C3H or 6291510 |
| AVDD | DVDD | Vref_INA | Vref | Vcc | Vee |
|---|---|---|---|---|---|
| 5.0V | 3V | 3.277V | 5.0V | 15V | –15V |
Instrumentation amplifiers are a common way of translating low-level sensor outputs to high-level signals to drive an ADC. Typically, instrumentation amplifiers are optimized for low noise, low offset, and low drift. Unfortunately, the bandwidth of many instrumentation amplifiers may not be sufficient to achieve good settling to ADC charge kickback at maximum sampling rates. This document shows how a wide-bandwidth buffer can be used with an instrumentation amplifier to achieve good settling at high sampling rates. Furthermore, many instrumentation amplifiers are optimized for high voltage supplies and it can be required to interface the high voltage output (that is, ±15V) to a lower voltage amplifier (for example, 5V). This design shows how a current-limiting resistor can protect the amplifier from electrical overstress in cases where the instrumentation amplifier is outside the input range of the op amp. A related cookbook circuit shows a simplified approach that does not include the wide-bandwidth buffer (Driving a Switched-Capacitor SAR With an Instrumentation Amplifier circuit design). The simplified approach has limited sampling rate as compared to the buffered design. Note that the following circuit shows a bridge sensor, but this method could be used for a wide range of different sensors.
This circuit implementation is applicable in applications such as analog input modules, electrocardiograms (ECGs), pulse oximeters, lab instrumentation, and control units for rail transport.
| Specification | Calculated | Simulated |
|---|---|---|
| Sampling rate | 1Msps | 1Msps, settling to –44µV |
| Offset (ADC Input) | 40μV × 306.7 = 12.27mV | 16mV |
| Offset Drift | (0.4μV/°C) × 306.7 = 123μV/°C | N/A |
| Noise | 978μV | 586μVRMS |



The following graph shows a linear output response for inputs from –5mV to +15mV. Refer to Determining a SAR ADC’s Linear Range when using Instrumentation Amplifiers for detailed theory on this subject. In cases where the INA826 output exceeds the op amp input range, the ESD diodes turn on and limit the input. The resistor R3 protects the amplifier from damage by limiting the input current (see the Overvoltage Protection Filter Between Instrumentation Amplifier and Op Amp section). The op amp output is inside the absolute maximum rating of the ADS8860 (–0.3V < VIN < REF +0.3V).
The bandwidth is simulated to be 11.45 kHz in this configuration. In this bandwidth it is not possible to drive the SAR converter at full speed. See the TI Precision Labs video series Op Amps: Bandwidth 1 for more details on this subject.
The OPA320 buffer (20MHz) is used because it is capable of responding to the rapid transients from the ADC8860 charge kickback. This type of simulation shows that the sample and hold kickback circuit is properly selected. Refer to Introduction to SAR ADC Front-End Component Selection for detailed theory on this subject.
Use a simplified noise calculation for a rough estimate. We neglect the noise from the OPA192 as the instrumentation amplifier is in high gain so its noise is dominant.

Note that the calculated and simulated match well. Refer to TI Precision Labs - Op Amps: Noise 4 for detailed theory on amplifier noise calculations, and Calculating the Total Noise for ADC Systems for data converter noise.
The filter between the INA826 and OPA320 serves two purposes. It protects the OPA320 from overvoltage, and acts as a noise or anti-aliasing filter. Scale the INA826 gain so that under normal circumstances, the output is inside the range of the OPA320 (that is, 0V to 5V). Thus, normally the overvoltage signals applied to the input of the OPA320 is not seen. However, during power up or in cases where the sensor is disconnected, the INA826 output can be at either power supply rail (that is, ±15V). In overvoltage cases, the resistor (R3) limits current into the OPA320 for protection. The internal ESD diodes on the OPA320 turns on during overvoltage events and direct the overvoltage signal to the positive or negative supply. In the following example, the overvoltage signal is directed to the positive supply and the transient voltage suppressor (D1, SMAJ5.0A) turns on to sink the current. Note that the resistor is scaled to limit the current to the OPA320 absolute maximum input current (10mA). See TI Precision Labs - Op Amps: Electrical Overstress (EOS) for detailed theory on this subject.

The following figure shows a commonly used instrumentation amplifier input filter. The differential noise is filtered with Cdif, and the common mode noise is filtered with Ccm1 and Ccm2. Note that it is recommended that Cdif ≥ 10Ccm. This prevents conversion of common mode noise to differential noise due to component tolerances. The following filter was designed for a differential cutoff frequency of 15kHz.

| Device | Key Features | Link | Similar Devices |
|---|---|---|---|
| ADS8860 | 16-bit resolution, SPI, 1-Msps sample rate, single-ended input, Vref input range 2.5V to 5.0V. | 16-bit, 1MSPS, 1-channel SAR ADC with single-ended input, SPI and daisy chain | Precision ADCs |
| OPA192 | 8-kHz bandwidth, Rail-to-Rail output, 450-nA supply current, unity gain stable | High-Voltage, Rail-to-Rail Input/Output, 5µV, 0.2µV/˚C, Precision Operational Amplifier | Precision op amps (Vos<1mV) |
| INA826 | Bandwidth 1MHz (G=1), low noise 18nV/rtHz, low offset ±40µV, low offset drift ±0.4µV/°C, low gain drift 0.1ppm/°C. (typical values) | Precision, 200-μA Supply Current, 36-V Supply Instrumentation Amplifier | Instrumentation amplifiers |
Link to Key Files
Texas Instruments, source files for SBAC184, software support