SBAA651 October   2024 TX7364

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction of TX7364 and Key Specifications
  5. 2Existing Design
  6. 3Advantages of TX7364 over TX7332
  7. 4New Reference Design with TX7364
  8. 5Benefits of New Design
  9. 6Summary
  10. 7References

Summary

This application note explores the advantages of a new reference design aimed for the portable ultrasound systems. The application note goes on to show how adopting one of TI's latest ultrasound transmitter, TX7364 has several advantages over the existing design that uses TX7332. The application note highlights the advantages TX7364 has over TX7332, and how using the design in the EVM design can bring down the board area, cost, and improving the overall simplicity of the layout as compared to the existing design.