SBAU206B april 2015 – may 2023
As noted in Section 1 and Section 2, the EVM interfaces with the PHI and communicates with the host over USB. Figure 4-1 shows how the PHI communicates with two devices on the EVM: the ADS1263 using the serial peripheral interface (SPI) and the EEPROM using the inter-integrated circuit (I2C) interface. The EEPROM comes preprogrammed with the information required to configure and initialize the ADS1263EVM. When the hardware is initialized, no further communication with the EEPROM is necessary and this device can be ignored by the user.
The ADS1263 uses SPI serial communication in mode 01 where CPOL = 0 and CPHA = 1. Header J2 in Figure 4-1 provides test points for all digital signals to and from the PHI controller. The test points can be connected to a logic analyzer for convenient visualization of the digital signals. These test points can also be used to communicate with the ADS1263EVM using an external controller.
Pullup resistor R22 drives the START pin high and puts ADC1 in continuous conversion mode. The ADC then continuously converts until the START pin is returned low. Pullup resistor R24 drives the RESET/PWDN pin high to hold the ADC in conversion mode. A momentary low pulse resets the ADC. Holding RESET/PWDN low enables the ADC power-down mode. Pullup resistor R35 brings the chip-select (CS) pin high, which resets the serial interface. The CS pin must be pulled low during the entire data transaction. More information about the specifics of the digital pins can be found in the ADS1263 data sheet.