SBAU206B april 2015 – may 2023
As noted throughout this document, the ADS1263 includes two ADCs: a 32-bit primary device (ADC1), and a 24-bit secondary converter (ADC2). The ADS1263EVM GUI is capable of controlling both ADC1 and ADC2 using the global settings on the left side of the GUI. Figure 7-7 highlights the controls for ADC2.
Figure 7-7 ADS1263EVM GUI Global Settings
for ADC2As Figure 7-7 shows, ADC2 can use a different data rate, gain, input channels, and reference voltage compared to ADC1. However, ADC2 can only use the Sinc3 filter, and both ADCs must use the same number of Samples. To view both ADC1 and ADC2 data in the GUI, select the Include ADC2 data? check box.
The GUI operates by converting samples at the data rate specified by ADC1, which can be different from ADC2. Therefore:
See the ADC2 section of the ADS1263 data sheet for more information about how to configure and retrieve data from ADC2.