SBAU416B November 2022 – January 2024 ADS9813
This section details the installation and operation of the ADS9813EVM and ADS9817EVM software graphical user interfaces (GUI). These softwares require the TSWDC155EVM (sold separately) controller to operate. The first step to installing the software (as shown in Figure 6-1) is to download the latest version of the EVM GUI installer as per Table 6-1.
EVM | Software Download Link |
---|---|
ADS9813EVM | ADS9813EVM-GUI |
ADS9817EVM | ADS9817EVM-GUI |
Accept all the license agreements and choose the destination location, project directory, and start menu. Typically, the default values work, but these values can be customized as needed based on the user's requirements.
Next, the installer prompts the user to create a desktop icon and summarize the installation plan. Clicking Install begins copying software onto the computer. This process takes a few minutes. At completion, the user can launch a readme text file and the application. Figure 6-2 shows these steps.