SBAU416B November   2022  – January 2024 ADS9813

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
    1. 1.1 ADS9813EVM and ADS9817EVM Features
  5. 2ADS9813EVM and ADS9817EVM Quick Start Guide
  6. 3Analog Interface
    1. 3.1 ADC Input SMA Connections
    2. 3.2 Voltage Reference
  7. 4Digital Interface and Clock Inputs
    1. 4.1 Digital Interface Connections
    2. 4.2 Clock Select
  8. 5Power Supplies
    1. 5.1 USB Power and When to Power the Board Externally
  9. 6ADS9813EVM and ADS9817EVM Software Reference
    1. 6.1 ADS9813EVM-GUI and ADS9817EVM-GUI Software Installation
    2. 6.2 USB Driver Installation
    3. 6.3 Using the CONFIG Tab
    4. 6.4 Using the Capture Tab
    5. 6.5 Using the INL/DNL Tool
    6. 6.6 Using the Histogram Tab
  10. 7Schematics, Layouts, and Bill of Materials
    1. 7.1 Schematics
      1. 7.1.1 ADS9813EVM Schematics
      2. 7.1.2 ADS9817EVM Schematics
    2. 7.2 Layout
    3. 7.3 Bill of Materials (BOM)
      1. 7.3.1 ADS9813EVM Bill of Materials (BOM)
      2. 7.3.2 ADS9817EVM Bill of Materials (BOM)
  11. 8Revision History

ADS9813EVM-GUI and ADS9817EVM-GUI Software Installation

This section details the installation and operation of the ADS9813EVM and ADS9817EVM software graphical user interfaces (GUI). These softwares require the TSWDC155EVM (sold separately) controller to operate. The first step to installing the software (as shown in Figure 6-1) is to download the latest version of the EVM GUI installer as per Table 6-1.

Table 6-1 EVM GUI Installers
EVMSoftware Download Link
ADS9813EVMADS9813EVM-GUI
ADS9817EVMADS9817EVM-GUI

Accept all the license agreements and choose the destination location, project directory, and start menu. Typically, the default values work, but these values can be customized as needed based on the user's requirements.

Note: The GUI installer and GUI buttons can differ slightly depending on which specific GUI is being installed.
GUID-20221025-SS0I-3KK0-S6GF-DJ14P0GWSCXV-low.pngFigure 6-1 Initial Software Installation

Next, the installer prompts the user to create a desktop icon and summarize the installation plan. Clicking Install begins copying software onto the computer. This process takes a few minutes. At completion, the user can launch a readme text file and the application. Figure 6-2 shows these steps.

GUID-20221025-SS0I-T2HL-D87D-NWDMC0C4NXB4-low.pngFigure 6-2 Installation Process