SBOS092C June 1998 – January 2026 XTR106
PRODUCTION DATA
The XTR106 is a monolithic 4mA-to-20mA, 2-wire current transmitter with a differential voltage input. Figure 6-1 shows the simplified schematic of the XTR106. The loop power supply, V+, provides power for all circuitry. The output loop current is modulated by the XTR106 and is typically measured as a voltage across a series load resistor (RL).
The instrumentation amplifier input of the XTR106 measures the voltage difference between the noninverting and inverting inputs. This difference is then gained up according to the value of RG, and expressed as a regulated current output.
Figure 6-1 Simplified Schematic