SBOS998E June 2021 – March 2026 BUF802
PRODUCTION DATA
The specified input-referred voltage noise of the BUF802 (see Section 5.5) is 2.3nV/√Hz. The total input referred RMS noise in a bandwidth of 1GHz is given by the following equation:
1.22 = Brick-wall correction factor. See TI Precision Labs – Op Amps: Noise – Spectral Density for detailed calculations.
Figure 8-3 shows the total input-referred spot noise as a function of frequency. Assuming the oscilloscope has eight divisions on the screen and a highest resolution of 1mV, the full-scale reading is 8mVPP or 2.82mVRMS. Thus, the SNR of the front-end amplifier stage at the highest-resolution setting is:
The parasitic input capacitance of BUF802 (IN pin) is 2.4pF. At 1GHz, this parasitic capacitance reduces to an impedance of 66.3Ω. Thus, the net input impedance seen by the signal at the input is:
This result is an imperfect termination for the 50Ω source, resulting in a poor S11. The addition of a 30Ω resistance in series with the input trace, and a 6.8nH inductor in series with the on-board 50Ω termination help isolate the input parasitic capacitance. This configuration also helps maintain the net input impedance at 50Ω. Figure 8-4 shows the S11 response of this modified circuit.
CL Mode of the BUF802 simplifies this design for achieving a flat frequency response from DC until the frequency of interest (1GHz in this case). To achieve a flat response, meet the following two conditions:
where
G varies from device-to-device; therefore, trim either α or β to achieve a flat frequency response. In Figure 8-1, trim β using the RPOT.
G is the typical value, (G = 0.971V/V) from Section 5.5 and
Therefore, trim RPOT so that β ≅ 1/5.
For the β network, use resistors that are an order of magnitude of resistance lower than the resistors used in the α network. Therefore, β resistor values of 80 kΩ and ≅ 20kΩ are chosen.
fHF is the pole resulting from the 330pF series capacitor and the 10MΩ resistor on the In_Bias pin. Reduction in value of 10MΩ helps with the reduction of overdrive recovery time of the composite loop, but increases the fHF pole frequency.
fLF is the pole resulting from the gain bandwidth of the precision amplifier (OPA140), the auxiliary path bandwidth and other parasitic capacitance of the resistor network.
where
The common mode input capacitor of the precision amplifier (CINPA) forms a pole with the Rα2 resulting in pole frequency of:
Since fLF2 < fLF1, fLF2 is considered as the dominant pole for the auxiliary path bandwidth. Based on the above value of fHF and fLF2, the required condition of fHF << fLF2 is met.
CF, connected across the precision amplifier, is required to compensate for the parasitic capacitance and to make the overall poles and zeros cancel each other. Use the following equation to find the value of CF:
where
Plugging in the value of these components arrives approximately to CF = 61pF, rounding off to nearest standard capacitor CF = 56pF. In the final system, based on the quality of the flat-band response needed, CF is able to be trimmed along with RPOT in the final production flow.