SBOSA39A April 2025 – October 2025 THS3470
PRODUCTION DATA
The THS3470 output current flags, ISNK_FLAG and ISRC_FLAG, are used to monitor when the current limits set by ISNK_LIMIT and ISRC_LIMIT and are met or exceeded on the VOUT pin of the device. If the ISNK_LIMIT current sinking limit (current entering the device output) is exceeded, the ISNK_FLAG pin is pulled low to DGND. If the ISNK_LIMIT current sinking limit is not exceeded, the ISNK_FLAG pin is pulled high to the internal VDD voltage of 5V. If the ISRC_LIMIT current sourcing limit (current exiting the device output) are exceeded, the ISNK_FLAG pin is pulled low to DGND. If the ISRC_LIMIT current sourcing limit is not exceeded, the ISNK_FLAG pin is pulled high to the internal VDD voltage of 5V.
There are two primary use cases for the output current flags. The first use case is to connect the ISNK_FLAG to the ISNK_LIMIT_EN pin to allow the device to self-limit the current into VOUT. The second use case is to connect ISNK_FLAG to a digital input/output pin of a microcontroller and monitor the pin as a current-warning flag. For more information regarding each of these use cases, see also Section 6.3.2.