SBOU034B February 2006 – October 2025 XTR300
The XTR300 has an internal instrumentation amplifier that can be used to monitor the output voltage when in current mode operation by looking at the IAOUT pin. The IAOUT pin has a transfer function as shown in Equation 3.
By default, the RG resistor is set to 10kΩ.
To convert IAOUT to a voltage, a resistor (R14) is used as seen in Equation 4. By default R14 is 750Ω.
The test point labeled IAOUT allows for easy to read monitoring of the IAOUT pin.