SBOU157 September 2015
The parameter list box gives the low-level register access. Usually this window is unused. Advanced users can adjust these parameters for optimal operation. Users wishing to use these registers are strongly encouraged to first read the Introduction to Time of Flight Camera – An Introduction, and the Introduction to the ToF System Design (SLOA190), and the Time-of-Flight Controller (TFC) data sheet of your specific camera, such as OPT9221. The parameter values can be saved to a *.csv file by clicking on the “floppy disc” icon at the upper right-hand corner.