SBOU274A December 2021 – January 2022
A liveview GUI window is launched when running the devInit.py script. This allows data from the OPT3004 to be viewed on a graph in real time. The GUI is created in the launchGUI.py example script. When running devInit.py, the launchGUI.py script is automatically run. However, if the GUI window is closed it can be re-launched by directly running the launchGUI.py script. To do this, select the launchGUI.py script and click Run>Buffer or press F5. Figure 3-13 shows the live GUI plot.