SBOU274A December 2021 – January 2022
When Latte is launched the GUI window appears front and center. However, there is a second window that is minimized at launch. This is the scripts window and exposes some more advanced features of the Latte platform. See Figure 3-14 .
Figure 3-14 Latte
Scripts WindowThe scripts window also provides access to the device registers view that displays the stored value of the device registers and allows them to be changed directly. Launch the registers view by double clicking on the "Registers View" button under the "Device List" box on the right side of the screen.
Figure 3-15 Registers
View