SBOU298B March 2024 – October 2026
Use the serial COM port to read and write registers through USB commands using the following format:
Set device address format: setdevice DEVID
Where setdevice is always lower case, and DEVID is defined as:
The 4LSBs of the device address in decimal format. For example, an address of 0x4A is 10.
Note, when the SCB is reset while one or more EVMs are connected, the address defaults to the lowest address found.
The SCB checks for I2C or SPI at start up. If no device is attached, then the device defaults to SPI. Reset the SCB with an I2C EVM connected to use I2C.
For example, to set the INA423XEVM with a register address of 0x4A, send the command: setdevice 10
For this example, the EVM returns the acknowledgment and state (idle or collecting) in JSON format: